text.skipToContent text.skipToNavigation
fast loop module

Swagelok® Fast Loop Modules

Swagelok fast loop modules are designed for handling long transport lines from tap to analyzer, providing minimum pressure drop for fastest response time. Interlocking handles on our fast loop sampling system solution help prevent incorrect sequencing of operation and accidental actuation.

Get In Touch with a Specialist

The Swagelok fast loop module (FLM) is designed to handle high flows and long transport lines from tap to analyzer to reduce time delays for online analyzer systems. Located at the analyzer shelter and offering a bypass, the Swagelok FLM easily isolates the sample system while introducing a purge gas for system cleaning. It then extracts a sample through a filter while using the high flow rate to keep the filter element clean.

Designed to enable easy access to any component without disturbing other components in the system, the Swagelok FLM uses welded assemblies to reduce potential leak points and zero-clearance fittings in straight run tubing sections.

The Swagelok FLM includes two ball valves that switch flow to a bypass to isolate the sample system and analyzer during maintenance. These bypass valves maintain flow through the fast loop to keep the sample fresh at the bypass point. An innovative interlocking handle system allows for simultaneous actuation of the valves, while allowing for packing adjustments within an individual valve body. In some configurations, the drain and purge valves are locked into the bypass valves to eliminate the possibility of opening the drain or purge lines while the system is in sample mode. All handles can be locked into position to eliminate the possibility of accidental actuation.

Fast Loop Sampling System

Sample transport lines are commonly more than 100 feet (30 meters) of tubing or pipe and require high purge volumes to ensure a fresh sample reaches the analyzer. Ideally, the flow from the sample tap to the analyzer shelter should take one minute or less. Depending on the tubing or pipe size of the transport lines, as well as the actual transport distance, this flow rate could be as high as 90 std ft3/h (2548 std L/h).

Minimize Sample Waste

A bypass filter specially designed for fast loop systems enables the FLM to provide high flow rates. The filter bypasses much of the sample flow and returns it to the process line through a secondary transport line. To generate high flow rates through this bypass loop, the return point must be at a lower pressure than the extraction point. Many Swagelok FLM configurations offer a sample return line from the analyzer to eliminate sending any continuous flow from an online analyzer to flare or disposal.

Virtually Eliminate Water Hammer

Closing a valve in a high-flow liquid line causes extreme pressure spikes, referred to as water hammer, which can damage system components. The Swagelok FLM eliminates the possibility of water hammer by making full shutoff impossible. The bypass valves actuate simultaneously to eliminate the possibility of actuating only one of the valves. The three-way valve design allows flow to switch gradually from sample mode to bypass mode, instead of temporarily shutting off during actuation.

View All of Our Sampling Videos

Fast Loop Module Catalogs

Locate detailed product information, including materials of construction, pressure and temperature ratings, options, and accessories.

Swagelok design and assembly services

Custom Fabrication for All Industries

Learn how Swagelok-trained specialists can save you time and improve your fluid system performance by designing and assembling systems for you.

Find the Support You Need

Swagelok Resources Curated for You

Analytical instrumentation panel with Swagelok valves and gauges
Tips to Maintaining a Representative Sample in an Analytical Instrumentation System

Maintaining a representative sample within an analytical instrumentation system can be difficult. Learn how to identify major issues and avoid complications associated with a compromised representative sample from the experts at Swagelok.

沈鼓集团股份有限公司的一名员工使用由世伟洛克部件构建的流体系统
沈鼓集团股份有限公司是如何提高系统安全性和可靠性的呢?

了解世伟洛克(上海)流体系统科技有限公司是如何帮助沈鼓集团股份有限公司在实现产品的一致性、可靠性和成本节省的同时,提高客户自身安全性和生产效率的。

Сотрудничество компаний Rosendahl Nextrom и Swagelok для оптимизации производства работ
Производитель оптоволоконного оборудования повышает эффективность через индивидуальные технические решения

С 1980-х годов Rosendahl Nextrom активно использует продукцию Swagelok для развития своего бизнеса. Узнайте больше о решениях, которые позволили компании опередить конкурентов и сохранить лидерство в отрасли.

Реализация проекта: компания Charbonneau Industries ускоряет производство с помощью специализированных узлов Swagelok для жидкостных и газовых систем
Ускорение производства с помощью специализированных узлов для жидкостных и газовых систем

Узнайте, как отдел специализированных решений Swagelok позволил компании Charbonneau Industries ускорить производство, сократить трудозатраты и обеспечить качество систем благодаря готовым системам перепускных термоклапанов.

请稍候几分钟,不要关闭此页面