text.skipToContent text.skipToNavigation
世伟洛克不锈钢球阀

世伟洛克® 阀门

世伟洛克阀门可在广泛的工作压力、温度和运行条件下可靠地控制流体,因此在关键的工业应用中,其能提供无泄漏且持久的运行性能,备受用户信赖。

查看阀门

世伟洛克阀门以其卓越的设计质量和耐用性而闻名,这些特性源于对材料采购和制造工艺的严格把控。即使在要求苛刻的应用中使用多年,世伟洛克阀门依然能够可靠地运行。我们对生产的每一个阀门都进行了严格的测试,以确保其符合我们的质量标准,因此您尽可放心,这些阀门将在您的最终使用环境中按需提供长期稳定的性能。

世伟洛克阀门具有以下特点:

  • 拥有多种端接,包括可检测的世伟洛克卡套管接头
  • 提供多种材料,使您能够找到与操作工作条件和流体相容的产品
  • 提供标准和适用于高纯和超高纯 (UHP) 应用的特殊清洁选项,以及获得了 API 的低排放认证

查阅我们的 PFAS 参考指南,深入了解全氟和多氟烷基物质 (PFAS) 以及世伟洛克产品中可选的阀座及密封件材质。

通过由近 200 个授权世伟洛克销售和服务网点组成的全球网络,您可以获得选择适合您应用的阀门、接受安装和维护培训方面的帮助,或获得故障排除方面的协助。

观看我们的阀门视频

是否想获取阀门选型和操作建议?

Valves Categories

Process Interface Valves (DBB)

Process Interface Valves (DBB)

确保在狭小空间内从工艺管道顺利过渡到仪表,同时尽可能地减少潜在泄漏点。

阀门目录

查找详细的产品信息,包括结构材料、额定压力和温度、选购件及配件。

Swagelok flow coefficient (C<sub>v</sub>) calculator for valves

Calculate Flow Rate for the Right Valve Selection

Use our valve flow coefficient (Cv) calculator to chose a valve sized correctly for your needs.

Use the Tool

Swagelok Resources Curated for You

Valve selection for  fluid sampling systems
How to Select the Right Valves for Your Industrial Fluid System

Learn how to apply the practical STAMPED method to select the valves most suited to your industrial fluid or sampling system design applications.

Reducing fugitive emissions in the chemical and refining industries
Minimize the Costs of Fugitive Emissions with Low-E Valves

Fugitive emissions are a growing concern in the chemical and petroleum refining industry. Certified low-emissions (Low-E) valves can protect your facility and bottom line. Learn what they are, how they are tested, and how they can help you in this post.

Block valves in an industrial fluid system
How to Isolate Industrial Fluid Systems with Block Valves

The isolation of industrial fluid system lines prior to maintenance is vital to plant safety. One of the safest ways to isolate a fluid system line is to install two block valves. Learn how to design proper configurations for your system.

Cleanroom assembly of a Swagelok ALD20 UHP valve for semiconductor industry use
One New Valve. Three Reasons It Could Change Semiconductor Manufacturing

Find out how the latest innovation in atomic layer deposition (ALD) valve technology is changing the game for high-tech semiconductor manufacturers.

Swagelok 60 series valve

Valves

Swagelok offers a variety of valves for industrial fluid systems—including ball valves, bellows-sealed valves, check valves, diaphragm valves, metering valves, needle valves, process interface valves, plug valves, quick connects, and relief valves—giving customers access to the solutions they need to achieve reliable flow control.

请稍候几分钟,不要关闭此页面