text.skipToContent text.skipToNavigation
gas distribution systems

Swagelok® Gas Distribution Systems

Gas distribution is a critical function for many industrial, research, and production facilities. Safely, reliably, and effectively delivering gases to where they are needed provide the foundation for a strong operation. Gas distribution systems work to deliver gases from a high-pressure source to the facility at the pressure and flow rate required by each application.

Contact a Specialist

Swagelok standard gas distribution panels come fully assembled and tested. They are easy to order from our application guide as single part numbers, minimizing the time your engineers spend on specification and procurement of new systems.

Swagelok modular panels feature minimal threaded connections to reduce potential leak points, and they are intuitively labeled to promote safe, simple use, and maintenance, and are backed by the Swagelok Limited Lifetime Warranty.

Learn more about Swagelok® Gas Distribution Systems

Swagelok gas distribution systems are built around one or a series of pressure regulation steps, and may include four subsystems:

Swagelok® Source Inlet (SSI)

The source inlet establishes a connection between the high-pressure gas source and the distribution system. It is important the inlet is built with appropriate cylinder connections, hoses, tubing, filters, and vent, purge, and relief functions to ensure that gas can be safely fed into the primary gas pressure control or automatic changeover. For a single gas cylinder, the assembly can be as simple as a hose and connector, while multiple cylinders may require a manifold incorporating many hoses and valves. Swagelok offers highly configurable options to purge or vent gases when changing bottles, always ensuring operator safety, as well as an available option to vent individual lines to maximize uptime.

Swagelok advisors will ensure all componentry is included and correctly specified with minimal connection points, hoses that do not drop to the ground, and properly supported components. Additionally, we can advise when certain gases may require the use of special hoses.

Swagelok® Gas Panel (SGP)

The SGP completes the first pressure reduction of the source gas and ensures it is delivered at the correct flow rate to the next stage of the system. Pressure reduction is accomplished in either one stage with a single pressure regulator or two stages through a dual pressure regulator arrangement.

Swagelok offers modular panels that are easy to service as any part can be detached via a Swagelok connection, so the panel never needs to be removed, as well as options implemented around the regulator and valves for color-coding if required for your site. Swagelok can also help you understand where a two-stage regulator is required.

View SGP Demonstration

Swagelok® Changeover (SCO)

The automatic changeover system seamlessly switches from one gas source to another to ensure an uninterrupted supply. This is accomplished through staggered set points of two pressure regulators, allowing the system to continue to operate as the primary gas source is changed. The changeover station allows for specified changeover set points to reduce wasted gas left in cylinders.

Swagelok offers more assurance the changeover point remains constant, as well as optional line regulation if your system incorporates a point of use regulator downstream—this can eliminate the additional cost of a regulator on the SCO. Swagelok specialists can help your team better understand system functionality, troubleshoot, and maintain operations.

Watch SCO Demonstration

Swagelok® Point-of-Use (SPU)

The point-of-use provides the critical last stage of pressure control prior to the gas being used. These typically have a pressure regulator, gauge, and isolation valve. Point-of-use systems offer a convenient and accurate method of adjusting pressure to meet test bench or equipment needs.

Swagelok offers standardization and consistent operation at the point-of-use; flat plate, bottom mount, top mount, and wall mount options; and a compact design. A Swagelok specialist can show you hidden savings, like how a single-stage SGP can be used to minimize cost where varying line pressure between the SGP and SPU is acceptable.

View SPU Demonstration

ガス供給システム・アプリケーション・ガイド

アセンブリーに関する詳細情報につきましては、以下の資料をご参照ください。

スウェージロックのガス供給システム評価/アドバイス・サービス

産業用ガス供給システムを理解する

オペレーションの効率化を図るには、産業用ガス供給システムの効率に直接影響を与える設計要素(利便性や保守性など)を知ることが大切です。

ホワイト・ペーパーを読む

関連資料/コラム記事

スウェージロックのガス供給ソリューションによる英国化学会社のガス・ライン最適化
導入事例:200本のガス・ライン。1つの包括的なソリューション。

英国のある大手化学薬品会社では、さまざまな特殊ガスを使用して研究開発を行っています。この会社は、 スウェージロックのガス供給システム・プログラムを活用することで、システムの安全性向上、ならびに新たな効率性を実現しました。

ガス供給パネルを検査するスウェージロックのエンジニア
ガス供給システムやパネルを改善してメンテナンス・コストを削減するには

取り扱いが容易なガス供給パネルや全体効率が高いガス供給システムを使用することで、分析室や精油所といった施設のメンテナンス・コストを削減する方法を紹介します。

ガス供給パネルを検査するスウェージロックのエンジニア
Q&A:効率的にガスを供給し、コストの削減や安全性の向上を実現するには

重要なガス供給システムの安全性と効率性の障害となる一般的な問題にはどのようなものがあるのか、また専門スタッフによるシステム評価によって得られる長期的な価値について紹介します。

ガス供給システムを検査するスウェージロックのエンジニア
ガス供給システムの安全性と効率性を向上させるために

研究室や試験設備、工業施設において、最大効率でオペレーションを行うには、ガス供給システムが非常に重要となります。今回は、ガス供給システムの健全性/安全性の最適化、コスト削減、ビジネスの成功に導く装置について紹介します。

This process may take several minutes. Please be patient and remain on the page.